iWave's WEC7 BSP Demo on Freescale's i.MX6 SABRE SDP/SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iWave's WEC7 BSP Demo on Freescale's i.MX6 SABRE SDP/SDB

iWave's WEC7 BSP Demo on Freescale's i.MX6 SABRE SDP/SDB

iWave Systems has made Windows Embedded Compact 7 (WEC7) available for Freescale’s i.MX6 SABRE SDP/SDB. All the latest features that WEC7 offers such as Silverlight 3.0, MPEG-4 HD, Expression Blend, Active Sync and also Adobe Flash10.1 are made available on this platform. The WEC7 BSP release supports SATA 3.0, Standard SD, Gigabit Ethernet, LVDS, Touch Panel, HDMI port and also necessary hardware codecs supported by the CPU. Debugging tools like KITL and CETK are also supported.

Comments

Very Good Demo!!! Impressive!!!

No ratings
Version history
Last update:
‎11-29-2012 08:00 PM
Updated by: