Yocto BSP for i.MX6 Pico-ITX SBC

cancel
Showing results for 
Search instead for 
Did you mean: 

Yocto BSP for i.MX6 Pico-ITX SBC

No ratings

Yocto BSP for i.MX6 Pico-ITX SBC

iWave released the official Yocto BSP for its i.MX6 Pico-ITX SBC board (iW-RainboW-G15S). The release is based on Linux 3.10.17 kernel and supports the following features:

  • i.MX6 ARM Cortex A9 Quad, Dual, Dual Lite & Solo CPU
  • 1GB DDR3 RAM (Quad, Dual, Dual Lite CPU version)/ 512MB DDR3 (Solo CPU version)
  • Freescale PMIC
  • SPI NOR Flash (default boot)imx6-pico-itx-single-board-computer
  • eMMC Flash (default OS storage)
  • Data UART
  • uSD slot
  • Standard SD slot
  • USB 2.0 Host
  • USB 2.0 device
  • 10/100/1000 Ethernet
  • Mini PCIex1 Port
  • CAN Port
  • LVDS display port
  • 4 Wire Resistive touch
  • PWM for backlight
  • HDMI Port with Audio
  • Hardware Codecs (Encode/Decode)
  • 2D/3D Graphics
  • CMOS CSI camera port
  • MIPI CSI camera port
  • AC97 Audio In/Out
  • Console UART
  • I2C Port
  • DIP Switch, Status LEDs (GPIOs)

This release supports single BSP, Binary image & MFG tool for all the four i.MX6 CPU version (Quad/Dual/Dual Lite/Solo) based SBC boards.

Besides this Linux BSP support, Android Jelly Bean and WEC7 board support packages also supported for the i.MX6 Pico SBC boards by iWave systems. More details about the i.MX6 Pico SBC board hardware & software features can be found in the following i.MX6 Pico SBC product page:http://www.iwavesystems.com/product/single-board-computer/i-mx6-pico-itx-sbc/i-mx6-pico-itx-sbc.html

Labels (1)
Version history
Revision #:
1 of 1
Last update:
‎05-20-2015 01:58 AM
Updated by: