SoM Summary Version - Nov/Dec 2013

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SoM Summary Version - Nov/Dec 2013

SoM Summary Version - Nov/Dec 2013

The Solution of the Month is the

Freescale i.MX6 based Qseven QMX6

a collaboration by Adeneo Embedded and congatec AG


Adeneo Embedded is proud to announce its collaboration with congatec on the Freescale i.MX6 based Qseven QMX6 computer-on-module.

Congatec is a leading supplier of industrial computer-on-modules supporting the ETX, XTX, COM Express and Qseven form factors.  The conga-QMX6 module was designed to the industry standard Qseven form factor. congatec’s products can be used in a variety of industries and applications, such as industrial automation, medical technology, automotive supplies, aerospace and transportation. Following the design-in phase, customers are given support via extensive product lifecycle management.

 

Adeneo Embedded has jointly developed and maintains Windows Embedded Compact, Linux and Android BSPs for the conga-QMX6 Qseven module. The combined expertise of both companies on h/w and s/w provides unmatched support to customers in enabling them to move quickly with their designs.

 

Adeneo Embedded continuously updates the BSP with feature updates and improvements. More information about this product and also other Freescale products supported by Adeneo Embedded can be found at http://www.adeneo-embedded.com/Products/Board-Support-Packages/Congatec-conga-QMX6-BSPs

Contact Adeneo Embedded @ sales@adeneo-embedded.com

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎07-29-2013 10:54 AM
更新者: