Dual camera & dual display working on MYIR's MYD-JX8MX Dev Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dual camera & dual display working on MYIR's MYD-JX8MX Dev Board

Dual camera & dual display working on MYIR's MYD-JX8MX Dev Board

MYD-JX8MX development board based on NXP i.MX8M quad processors provides powerful multi-media functions including dual displays, dual cameras, high-quality audio, etc. The target applications scale from consumer home audio to industrial building automation and mobile computers requiring high-performance and low-power processors.

Highlights:

- MYC-JX8MX CPU Module as Controller Board

- NXP i.MX 8M Quad Application Processor

- 1GB / 2GB LPDDR4, 8GB eMMC Flash, 256Mbit QSPI Flash

- RS232, 4 x USB 3.0 Host, 1 x USB 3.0 Host/Device, PCIe 3.0 (x4) NVMe SSD Interface, TF Card Slot

- Supports Gigabit Ethernet, WiFi/BT and 4G LTE - 2 x MIPI-CSI, HDMI, 2 x LVDS, MIPI-DSI, Audio Input/Output

标签 (1)
无评分
版本历史
最后更新:
‎06-13-2019 09:22 PM
更新人: