The BD-SL-i.MX6 formerly SABRE Lite board is a low cost i.MX6 development platform. One of the best attributes of the board is the significant software support that is available. This post introduces Qt5.4 from the QT Company. The video below shows The Qt Company’s enterprise device creation offering, a Qt-optimized pre-built software stack that lets you immediately get started with prototyping on a real device for embedded Linux and Android development. The demo is running Qt5.4 and the image is available for the BD-SL-i.MX6 as well as our Nitrogen family of products. Here is a brief video showing some of the capabilities:
The video above showed an image created for embedded Linux, and more specifically, built using tools from The Yocto Project and The Freescale Community BSP. Because of this, your products can leverage the packages provided by those projects, and you can use the Yocto build system to integrate your components and tailor your build.
For more details, visit http://qt.io or http://boundarydevices.com/qt-for-device-creation/