Apalis iMX6: Latest addition to Toradex' Apalis Family of ARM Computer Modules

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Apalis iMX6: Latest addition to Toradex' Apalis Family of ARM Computer Modules

Apalis iMX6: Latest addition to Toradex' Apalis Family of ARM Computer Modules

Toradex is thrilled to announce the arrival of the newest member in its Apalis family of computer-on-modules, the Apalis iMX6. The module is based on Freescale i.MX 6 series of SoC, runs a quad-core ARM Cortex-A9 CPU, and offers an operating frequency of up to 1.2 GHz. Apart from the benefits of long term product availability (of more than 10 years), and compatibility with the existing Apalis T30 module, this module is also qualified for industrial temperature range -40° C to 85° C.

More details including datasheet shall be published by the last week of February. For a preliminary look at the datasheet, please click here.

For more details on Apalis family, click here.

To know more about the Apalis T30 module, click here.

Here's a first look at the module.

Apalis iMX6: image

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎02-13-2014 03:25 AM
更新者: