uuu failed to load u-boot in iMXRT105X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uuu failed to load u-boot in iMXRT105X

612 Views
juanjovicente
Contributor II

Hi,

I´m trying to load a u-boot image in an iMXRT1052 using uuu.

I´ve managed to include the RT105X family into uuu's "known processors". However, I get some libusb related errors when I plug the SoC in Serial Download mode:

pastedImage_1.png

Any advice on this? I´m using a virtual machine with Ubuntu 16.04. Can anybody help me checking if it works in a native Ubuntu machine?

Why there is no support for iMXRT105X family in uuu?

Thanks and regards,

Juanjo

0 Kudos
1 Reply

527 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Juan Jose Vicente

Unfortunately, as you mentioned, RT10xx device family is not supported in the uuu tool, and at the moment there isn't plan to add the support, you can use mfgtool and elftosb tools. You can also check the community post:

One-stop secure boot tool: NXP-MCUBootUtility is upgraded to v1.4.0 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos