uboot for 1060 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot for 1060 evk

500 Views
jautry
Contributor IV

Is there a uboot somewhere already built that can run on the 1060 EVK that can be loaded with the MFGTOOL?

0 Kudos
1 Reply

496 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is there a uboot somewhere already built that can run on the 1060 EVK that can be loaded with the MFGTOOL?
-- As I know, there's not a Uboot for i.MX RT MCU and it needs the developer to customize such a Uboot by himself
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos