sdk for imx rt1050 is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdk for imx rt1050 is not working

1,350 Views
wernerabbler
Contributor I
"SDK version 2.3.0 package for EVK-MIMXRT1050 board" is not found by Xpresso Config 3.0 tools. No CPU infos, Boards or examples are available. Is there a trick to get it working ?
Labels (1)
0 Kudos
1 Reply

1,121 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Werner,

MCUXpresso tools are not yet available yet for i.MX RT devices. MCUXpresso Pins and Clocks tool should be available by the end of November.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos