mbed support for RT1020 and LPC55S28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mbed support for RT1020 and LPC55S28

889 Views
kevin11
Contributor I

Hi,

Does NXP has any plan to support mbed OS on RT1020 and LPC55S28 platform ?

If no, please advise which example project that I can reference.

Thanks.

Labels (1)
Tags (3)
0 Kudos
1 Reply

756 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Kevin Chu,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Does NXP have any plan to support mbed OS on RT1020 and LPC55S28 platform?
-- Actually, the mbed OS is developed by ARM, we don't know the schedule of planning to support other LPC55Sxx and i.MX RT series MCU in addition to RT1050 and LPC55S69.
2) Do you have the plan to port Zephyr on LPC55S28 as well?
-- For NXP, we don't have the plan to provide the demo about the Zephyr OS in the SDK software library recently.
3)  If not, how can I port it by myself? Any guidelines or instructions will be appreciated.
-- Firstly, I consider the Zephyr OS is able to run on the LPC55S28 too, regard the porting flow, I'd highly recommend you to refer to the User and Developer Guides.
I hope it helps.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos