I'm trying to use MFGTool2 to load boot_image.sb onto HyperFlash of the IMXRT1050-EVKB. I followed every step in section 3.4 of the attached AN12107. I repeated multiple times to make sure I did not miss anything. But every time it failed to program the boot image.
I check the MfgTool.log. It gives me this error:
"description" : "10101 (0x2775) kStatusRomLdrSignature",
From the reference manual, this error means "ROM SB loader incorrect signature". But I don't know how I got this and what I did wrong.
Can anybody help please?
Thanks in advance,
Bin
Hello Bin Zhang,
What it comes to mind is that the SB file wasn't correctly created,
did you type in the cmd the correct line,(step 7 in AN12107)?
elftosb.exe -f kinetis -V -c ../../bd_file/imx10xx/program_flexspinor_image_HyperFlash.bd -o boot_image.sb ivt_flexspi_nor_hello_world_nopadding.bin
Regards,
Aldo.