kStatusRomLdrSignature when using MFGTool2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kStatusRomLdrSignature when using MFGTool2

1,104 Views
bzhang3
Contributor I

I'm trying to use MFGTool2 to load boot_image.sb onto HyperFlash of the IMXRT1050-EVKB. I followed every step in section 3.4 of the attached AN12107. I repeated multiple times to make sure I did not miss anything. But every time it failed to program the boot image. 

I check the MfgTool.log. It gives me this error:

   "description" : "10101 (0x2775) kStatusRomLdrSignature",

From the reference manual, this error means "ROM SB loader incorrect signature". But I don't know how I got this and what I did wrong. 

Can anybody help please?

Thanks in advance,

Bin

Labels (1)
0 Kudos
2 Replies

906 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello Bin Zhang,

What it comes to mind is that the SB file wasn't correctly created, 

did you type in the cmd the correct line,(step 7 in AN12107)? 

elftosb.exe -f kinetis -V -c ../../bd_file/imx10xx/program_flexspinor_image_HyperFlash.bd -o boot_image.sb ivt_flexspi_nor_hello_world_nopadding.bin

Regards, 

Aldo.

0 Kudos

906 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi again, 

I saw your previous threads,

could you tell me if you were able to create the bin file?

Regards,

Aldo.

0 Kudos