individual interrupt priority setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

individual interrupt priority setting

Jump to solution
908 Views
jinu_mohan
Contributor I

hi for setting interrupt priority setting  in IMXRT1060s we are using 

NVIC_SetPriority(GPIO6_7_8_9_IRQn, 4);

is there any method to set the individual priority of these combined interrupts

because currently we are using four interrupts in this combined irqn we need to set higher priority to one specific pin interrupt 

@kerryzhou 

Tags (1)
0 Kudos
1 Solution
900 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jinu_mohan ,

  Thanks for your trust!

  You mean, in the internal group:GPIO6_7_8_9_IRQn, whether you can set the individual priority, right?

   No, to this one, it share the IRQ.

  So, if you want to set the infividual priority, you need to use the different IRQ.

 You can use this GPIO:

kerryzhou_0-1650960553909.png

Then different pin has different IRQ, you totally can set it's own priority.

Wish it helps you!

Best Regards,

Kerry

 

 

View solution in original post

0 Kudos
1 Reply
901 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jinu_mohan ,

  Thanks for your trust!

  You mean, in the internal group:GPIO6_7_8_9_IRQn, whether you can set the individual priority, right?

   No, to this one, it share the IRQ.

  So, if you want to set the infividual priority, you need to use the different IRQ.

 You can use this GPIO:

kerryzhou_0-1650960553909.png

Then different pin has different IRQ, you totally can set it's own priority.

Wish it helps you!

Best Regards,

Kerry

 

 

0 Kudos