imxrt serial downloader issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt serial downloader issue

Jump to solution
202 Views
ancymuhammed
Contributor III

We are using iMXRT1176 for one of our project. USB1 is used for OTG (Serial downloader) and device. Whether USB1_VBUS has to be connected to 5V inorder to work as serial downloader. 

Currently programming is successful only after connecting 5V to VBUS of iMXRT. Whether this connection is mandatory. 

0 Kudos
1 Solution
188 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, it should be connected. If USB1 is unused then you can leave unconnected USB1_DN, USB1_DP, USB1_VBUS.

Best regards,
Omar

View solution in original post

0 Kudos
1 Reply
189 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, it should be connected. If USB1 is unused then you can leave unconnected USB1_DN, USB1_DP, USB1_VBUS.

Best regards,
Omar

0 Kudos