imxRT1050 and resistive touch screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxRT1050 and resistive touch screen

1,586 Views
giannigrondona
Contributor III

Hi

I have a resistive touch screen ( 4 wires)  and I have to connect it to imxRT1062. I know inside there is an interface for that kind of touch screen. Can I found an application note that show how to handle touch screen controller and ADC module ?

Best Regards

Giovanni Grondona

Tags (1)
0 Kudos
2 Replies

1,371 Views
joanxie
NXP TechSupport
NXP TechSupport

only one application note about eLCDIF, can connect NXP LCD extension board which supports touch panel

https://www.nxp.com/docs/en/application-note/AN12302.pdf 

0 Kudos

1,371 Views
giannigrondona
Contributor III

Hi Joanxie

In the application note AN12302 there is nothing about touch screen

controller. I have a resistive touch control and I have to connect my

LCD display and touch screen to microprocessor. No problem to connet LCD

signals (RGB) to microprocessor, the problem is about how to connect 4

wires of resistive touch control to microprocessor ( IMXRT 1050)

Thank you

Best Regards

Giovanni

Il 29/01/2019 06.22, joanxie ha scritto:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: imxRT1050 and resistive touch screen

reply from Joan Xie

<https://community.nxp.com/people/joanxie?et=watches.email.thread> in

/i.MX Processors/ - View the full discussion

<https://community.nxp.com/message/1106633?commentID=1106633&et=watches.email.thread#comment-1106633>

>

0 Kudos