Hello,
We just got today a new mimxrt1060 EVK.
It works fine with ram debug, but on configuring to spiflash it fails as following:
Wed Oct 31, 2018 17:22:14: IAR Embedded Workbench 8.30.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.1\arm\bin\armproc.dll)
Wed Oct 31, 2018 17:22:14: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.1\arm\config\debugger\NXP\iMXRT.dmac
Wed Oct 31, 2018 17:22:14: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.1\arm\config\debugger\NXP\iMXRT_Trace.dmac
Wed Oct 31, 2018 17:22:14: Loading the CMSIS-DAP driver
Wed Oct 31, 2018 17:22:14: Probe: CMSIS-DAP probe SW module ver 1.13
Wed Oct 31, 2018 17:22:14: Probe: CMSIS-DAP S/N '0229000005da88a000000000000000000000000097969905' mapped to a number 97969905.
Wed Oct 31, 2018 17:22:14: Emulation layer version 4.34
Wed Oct 31, 2018 17:22:15: Notification to init-after-power-up hookup.
Wed Oct 31, 2018 17:22:15: Notification to core-connect hookup.
Wed Oct 31, 2018 17:22:15: Connected DAP v1 on SWD. Detected IDCODE=0xbd11477.
Wed Oct 31, 2018 17:22:15: Probe: ConnectSpec='CMSIS-DAP:0229000005da88a000000000000000000000000097969905:7-3A81E2DE-0-0000'.
Wed Oct 31, 2018 17:22:15: Connecting to TAP#0 DAP AHB-AP port 0 (IDR=0x4770041).
Wed Oct 31, 2018 17:22:15: Recognized CPUID=0x411fc271 Cortex-M7 r1p1 arch ARMv7-M
Wed Oct 31, 2018 17:22:15: Set cacheable access on AHB-AP port 0 (HPROT=0xeb000000).
Wed Oct 31, 2018 17:22:15: Debug resources: 8 instruction comparators, 4 data watchpoints.
Wed Oct 31, 2018 17:22:15: MultiCore: Asynchronous core execution FORCED.
Wed Oct 31, 2018 17:22:15: MultiCore: Synchronous core execution DISABLED.
Wed Oct 31, 2018 17:22:15: LowLevelReset(hardware, delay 200)
Wed Oct 31, 2018 17:22:16: Notification to init-after-hw-reset hookup.
Wed Oct 31, 2018 17:22:16: Probe: ConnectSpec='CMSIS-DAP:0229000005da88a000000000000000000000000097969905:7-3A81E2DE-0-0000'.
Wed Oct 31, 2018 17:22:16: Connecting to TAP#0 DAP AHB-AP port 0 (IDR=0x4770041).
Wed Oct 31, 2018 17:22:16: Recognized CPUID=0x411fc271 Cortex-M7 r1p1 arch ARMv7-M
Wed Oct 31, 2018 17:22:16: Set cacheable access on AHB-AP port 0 (HPROT=0xeb000000).
Wed Oct 31, 2018 17:22:16: Debug resources: 8 instruction comparators, 4 data watchpoints.
Wed Oct 31, 2018 17:22:16: CPU status - IN RESET
Wed Oct 31, 2018 17:22:17: Loaded debugee: C:\Users\ransh\Downloads\SDK_2.4.0_EVK-MIMXRT1060 (3) (1)\boards\evkmimxrt1060\demo_apps\shell\iar\flexspi_nor_debug\shell.out
Wed Oct 31, 2018 17:22:17: Download error at 0x60000000: downloading into non-writable memory.
Wed Oct 31, 2018 17:22:17: Download error at 0x60001000: downloading into non-writable memory.
Wed Oct 31, 2018 17:22:17: Download error at 0x60002000: downloading into non-writable memory.
Wed Oct 31, 2018 17:22:17: Download error at 0x60002000: memory write failed.
* In ram debugging with IAR (same project , imxrt1060, sdk 2.4.0) - no issue. Only with spiflash debug in IAR.
* With mimxrt1050 (sdk 2.4.2) no issues in spinor debug with IAR.
* It seems that xip examples is for qspi (not hyperflash) .
On trying to use the imxrt1050 hyperflash files instead of qspi, there is an error on startup !
* We also tried to change switch state - sw 7 by default is for qspi, we changed it to spiflash - 0110 - yet, no change in behaviour. Maybe it's SW5 ? Wwhy sw5 is not mentioned in MIMX1060 user guide ?
Can anyone help with this ?
ranran
Hi ranran,
On the EVKB-MIMXRT1050 board, the HyperFlash is the default memory and it is required to apply a rework on the board to enable the QSPI Flash, however on the EVK-MIMXRT1060 is the opposite, the QSPI is the default memory and it is required to apply a rework on the board to enable the HyperFlash.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Carlos,
Can you please elaborate what change in board is required if we need to work with hyperflash instead of qspi ?
Thank you,
ranran
Hi,
It is explained on section 2.6 of MIMXRT1060 Evaluation Kit Board Hardware User's Guide:
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------