iMXRT1064 Hardware acceleration capabilities

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1064 Hardware acceleration capabilities

435 Views
anujtanksali
Contributor II

Hello,

I am currently using iMXRT1064 controller with Emwin graphical library and 800x480 7" LCD with RGB mode.

Does the iMXRT1064 support any hardware acceleration capability for drawing of bitmaps so that the drawing can be faster?

If not then are there any other options by which the drawing on the LCD can be made fast.

Thanks

Regards,

Anuj

 

 

 

0 Kudos
1 Reply

422 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Anuj,

Please refer to the application note below. In section 4.2 there are a few tips that can help you to improve performance.

https://www.nxp.com/docs/en/application-note/AN12302.pdf

Best regards,

Felipe

0 Kudos