iMXRT1021 change FlexRAM size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1021 change FlexRAM size

Jump to solution
662 Views
huy_tv
Contributor I

Dear all, 

I have a trouble with FlexRAM resize.
Following reference Reallocating-the-FlexRAM , i can change IMXRT1021 ram size (ITC-OC-DTC) from default (64KB-128KB-64KB) to new value (64KB-64KB-128KB).
After flash program with Jlink, device can success boot up, run application without any problems. 
When i call software reset (NVIC_SystemReset), device still booting up again and work fine.

But when i turnoff power source and turn on again, device never run to application success. Could you please give me your suggestion?
Thank you.

Edit1: With default RAM config, device can boot ok, booting problem only happen when i relocate FlexRAM

This is my configuration for relocate FlexRAM
1. Reset handler

 

 

void ResetISR(void) {

    // Disable interrupts
    __asm volatile ("cpsid i");

// For debug only
    volatile unsigned int IOMUXC_GPR_GPR17_Reg = *((unsigned int *) 0x400ac044);
    volatile unsigned int IOMUXC_GPR_GPR16_Reg = *((unsigned int *) 0x400ac040);
//

    /* Reallocating the FlexRAM */
    __asm (".syntax unified\n"

    "LDR R0, =0x400ac044\n" //Address of register IOMUXC_GPR_GPR17
    "LDR R1, =0x00005FAA\n" //FlexRAM configuration DTC = 128KB, ITC = 64KB, OC = 64KB
    "STR R1,[R0]\n"


    ".syntax divided\n");

    __asm volatile ("MSR MSP, %0" : : "r" (&_vStackTop) : );
...........
}

 

 


2. MPU config for new FlexRAM configuration

 

 

/* Region 4 setting: Memory with Device type, not shareable, non-cacheable. */
    MPU->RBAR = ARM_MPU_RBAR(4, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);

    /* Region 5 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(5, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64KB);

    /* Region 6 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(6, 0x20000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_128KB);

    /* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(7, 0x20200000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64KB);

    /* Region 8 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(8, 0x80000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);

 

 

 

3. Linker option

huy_tv_0-1627698630703.png

4. XIP Nor option

huy_tv_1-1627698768322.png

 

 

Labels (1)
0 Kudos
1 Solution
634 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to use the below code instead of the original one and give it a try again.

void ResetISR(void) {

    // Disable interrupts
    __asm volatile ("cpsid i");

 
    //FlexRAM reallocate: ITC-OC-DTC(64KB-64KB-128KB)
    FLEXRAM->TCM_CTRL = 4;
    IOMUXC_GPR->GPR17 = 0x0000FAA5;
    IOMUXC_GPR->GPR16 |= 0x7;
    IOMUXC_GPR->GPR14 =  (8<<20) | (7<<16) ;

#if defined (__USE_CMSIS)
// If __USE_CMSIS defined, then call CMSIS SystemInit code
    SystemInit();
#else
    // Disable Watchdog
    volatile unsigned int *WDOG1_WCR = (unsigned int *) 0x400B8000;
    *WDOG1_WCR = *WDOG1_WCR & ~(1 << 2);
    volatile unsigned int *WDOG2_WCR = (unsigned int *) 0x400D0000;
    *WDOG2_WCR = *WDOG2_WCR & ~(1 << 2);
    // Write watchdog update key to unlock
    *((volatile unsigned int *)0x400BC004) = 0xD928C520;
    // Set timeout value
    *((volatile unsigned int *)0x400BC008) = 0xFFFF;
    // Now disable watchdog via control register
    volatile unsigned int *RTWDOG_CS = (unsigned int *) 0x400BC000;
    *RTWDOG_CS = (*RTWDOG_CS & ~(1 << 7)) | (1 << 5);

#endif // (__USE_CMSIS)

    //
    // Copy the data sections from flash to SRAM.
    //
    unsigned int LoadAddr, ExeAddr, SectionLen;
    unsigned int *SectionTableAddr;

    // Load base address of Global Section Table
    SectionTableAddr = &__data_section_table;

    // Copy the data sections from flash to SRAM.
    while (SectionTableAddr < &__data_section_table_end) {
        LoadAddr = *SectionTableAddr++;
        ExeAddr = *SectionTableAddr++;
        SectionLen = *SectionTableAddr++;
        data_init(LoadAddr, ExeAddr, SectionLen);
    }

    // At this point, SectionTableAddr = &__bss_section_table;
    // Zero fill the bss segment
    while (SectionTableAddr < &__bss_section_table_end) {
        ExeAddr = *SectionTableAddr++;
        SectionLen = *SectionTableAddr++;
        bss_init(ExeAddr, SectionLen);
    }


#if !defined (__USE_CMSIS)
// Assume that if __USE_CMSIS defined, then CMSIS SystemInit code
// will setup the VTOR register

    // Check to see if we are running the code from a non-zero
    // address (eg RAM, external flash), in which case we need
    // to modify the VTOR register to tell the CPU that the
    // vector table is located at a non-0x0 address.
    unsigned int * pSCB_VTOR = (unsigned int *) 0xE000ED08;
    if ((unsigned int *)g_pfnVectors!=(unsigned int *) 0x00000000) {
        *pSCB_VTOR = (unsigned int)g_pfnVectors;
    }
#endif // (__USE_CMSIS)
#if defined (__cplusplus)
    //
    // Call C++ library initialisation
    //
    __libc_init_array();
#endif

    // Reenable interrupts
    __asm volatile ("cpsie i");

#if defined (__REDLIB__)
    // Call the Redlib library, which in turn calls main()
    __main();
#else
    main();
#endif

    //
    // main() shouldn't return, but if it does, we'll just enter an infinite loop
    //
    while (1) {
        ;
    }
}

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
635 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to use the below code instead of the original one and give it a try again.

void ResetISR(void) {

    // Disable interrupts
    __asm volatile ("cpsid i");

 
    //FlexRAM reallocate: ITC-OC-DTC(64KB-64KB-128KB)
    FLEXRAM->TCM_CTRL = 4;
    IOMUXC_GPR->GPR17 = 0x0000FAA5;
    IOMUXC_GPR->GPR16 |= 0x7;
    IOMUXC_GPR->GPR14 =  (8<<20) | (7<<16) ;

#if defined (__USE_CMSIS)
// If __USE_CMSIS defined, then call CMSIS SystemInit code
    SystemInit();
#else
    // Disable Watchdog
    volatile unsigned int *WDOG1_WCR = (unsigned int *) 0x400B8000;
    *WDOG1_WCR = *WDOG1_WCR & ~(1 << 2);
    volatile unsigned int *WDOG2_WCR = (unsigned int *) 0x400D0000;
    *WDOG2_WCR = *WDOG2_WCR & ~(1 << 2);
    // Write watchdog update key to unlock
    *((volatile unsigned int *)0x400BC004) = 0xD928C520;
    // Set timeout value
    *((volatile unsigned int *)0x400BC008) = 0xFFFF;
    // Now disable watchdog via control register
    volatile unsigned int *RTWDOG_CS = (unsigned int *) 0x400BC000;
    *RTWDOG_CS = (*RTWDOG_CS & ~(1 << 7)) | (1 << 5);

#endif // (__USE_CMSIS)

    //
    // Copy the data sections from flash to SRAM.
    //
    unsigned int LoadAddr, ExeAddr, SectionLen;
    unsigned int *SectionTableAddr;

    // Load base address of Global Section Table
    SectionTableAddr = &__data_section_table;

    // Copy the data sections from flash to SRAM.
    while (SectionTableAddr < &__data_section_table_end) {
        LoadAddr = *SectionTableAddr++;
        ExeAddr = *SectionTableAddr++;
        SectionLen = *SectionTableAddr++;
        data_init(LoadAddr, ExeAddr, SectionLen);
    }

    // At this point, SectionTableAddr = &__bss_section_table;
    // Zero fill the bss segment
    while (SectionTableAddr < &__bss_section_table_end) {
        ExeAddr = *SectionTableAddr++;
        SectionLen = *SectionTableAddr++;
        bss_init(ExeAddr, SectionLen);
    }


#if !defined (__USE_CMSIS)
// Assume that if __USE_CMSIS defined, then CMSIS SystemInit code
// will setup the VTOR register

    // Check to see if we are running the code from a non-zero
    // address (eg RAM, external flash), in which case we need
    // to modify the VTOR register to tell the CPU that the
    // vector table is located at a non-0x0 address.
    unsigned int * pSCB_VTOR = (unsigned int *) 0xE000ED08;
    if ((unsigned int *)g_pfnVectors!=(unsigned int *) 0x00000000) {
        *pSCB_VTOR = (unsigned int)g_pfnVectors;
    }
#endif // (__USE_CMSIS)
#if defined (__cplusplus)
    //
    // Call C++ library initialisation
    //
    __libc_init_array();
#endif

    // Reenable interrupts
    __asm volatile ("cpsie i");

#if defined (__REDLIB__)
    // Call the Redlib library, which in turn calls main()
    __main();
#else
    main();
#endif

    //
    // main() shouldn't return, but if it does, we'll just enter an infinite loop
    //
    while (1) {
        ;
    }
}

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
627 Views
huy_tv
Contributor I

Thanks Jery.

It's work

0 Kudos