iMXRT1021 QSPI Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1021 QSPI Boot

Jump to solution
739 Views
manuabraham
Contributor III

Greetings,

 

We would like to move the QSPI Flash from FlexSPI_A to FlexSPI_B.

Would like to have the clarification, before going in for that change.

Are there any known issues in doing so ?

 

Thanks,

 

0 Kudos
1 Solution
715 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

ROM does not support boot from FLEXSPI_B port directly. ROM always seeks a valid Flash Configuration Block from the
FLEXSPI_A port and then re-configures the FLEXSPI controller using the valid parameters in the block read-out. This reconfiguration can include but is not limited to, FLEXSPI_B port support.

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

View solution in original post

1 Reply
716 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

ROM does not support boot from FLEXSPI_B port directly. ROM always seeks a valid Flash Configuration Block from the
FLEXSPI_A port and then re-configures the FLEXSPI controller using the valid parameters in the block read-out. This reconfiguration can include but is not limited to, FLEXSPI_B port support.

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------