iMX.RT1050 dcdc can't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX.RT1050 dcdc can't work

1,156 Views
dingzhongkui
Contributor I

hello:

    In rare cases, iMX.RT1050 board dcdc can't work with the voltage is 0v. But under normal condition,the output is 1.25v with 528Mhz. Power up again the failure  is removed.It is a new developed board, I think the overcurrent is more possible . the datasheet metion that  dcdc has Over current protection,Over voltage protection and Low voltage detection。

1)Whether some register can record  the wrong time?

2)  DCDC Register 0  is  the settings as follows with reset。whether the 8/11/17 is open or closed?

捕获1111.PNG

3)whether it can close the the  overcurrent/ low voltage /high voltage or not ?  the setting is"1" is right?

捕获.PNG

0 Kudos
3 Replies

952 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

i.MXRT1050 power up required 1ms delay with DCDC_PSWITCH.

Please check picture for the detailed info:

pastedImage_2.png

Please refer below circuit design to add RC delay circuit at DCDC_PSWITCH pin.

I also recommend customer to add resistor or capacitor value to add delay time to DCDC_PSWITCH pin.

pastedImage_1.png

There couldn't record DCDC time.

If DCDC output voltage is 0V, the ARM core without power couldn't work.

There make no sense of DCDC register value.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

952 Views
dingzhongkui
Contributor I

Hi,Mike:

        I'm sorry that my expression is incomplete.The wrong is happened when the operation is normal,without power on.

0 Kudos

952 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Sorry for the later reply.

I still confusion with  your question.

Could you provide the detailed info about internal DCDC working status?

If you could share your board power related circuit? Thanks.

best regards,

Mike

0 Kudos