iMX-RT RAM requirement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX-RT RAM requirement

658 Views
vinayakaghor13
Contributor I

Hello,

I want to know if I use FRAM instead of SDRAM, then which functions I will not be able to use for IMX RT 1052

Regards,

Vinayak

Labels (1)
0 Kudos
1 Reply

563 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinayak

if FRAM timings are the same as SDRAM, there are no restrictions for IMX RT1052,

except probably FRAM life time.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos