i.mx rt1064 type1MW wiced using WiFi and BLE at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx rt1064 type1MW wiced using WiFi and BLE at the same time

843 Views
sheng_cao
Contributor II

Hi,

I have a i.mx rt1064 dev board connected with Murata 1MW module, and had successfully managed to get WiFi working.

Is it possible to use BLE and WiFi at the same time with through the WICE api? SDK 2.7.0 has a firmware image which allows passthrough BLE commands through UART but I believe it's not compatible with 1MW.

Would a 1DX module be able to communicate using WiFi and BLE at the same time using the example WICED FW image from wiced_bt_passthrough example?

Are there plans for integration of 1MW for WiFi and BLE in future SDKs? If not, would I be able to find the WICED FW source code so I can build it myself from WICED IDE?

0 Kudos
1 Reply

728 Views
romitchatterjee
Contributor V

I do not think RT 1064 supports BLE yet. You can try with the RT 1060 EVK - that is known to work with 1DX and have support for both Wi-Fi and BLE (you can check out the examples in the SDK).

As for support for 1MW, I believe it is not supported yet, but hopefully will soon be.