Hi,
i am trying to set 2 pins from 1 port, e.g. GPIO2.31 and GPIO2.29.
One pin should be set in an irq handler, the other one in my main loop.
therefore i used the register DR_SET and DR_CLEAR.
But the pins are not set or clear in real? Both pins are always 0. Do you have any idea to that?
When i use the DR register, then the pins are set correctly.
Thanx
Hi,
i tried the demo project "igpio_led_output". same problem here, dr_toggle does not work, LED is not blinking.
then undefined "FSL_FEATURE_IGPIO_HAS_DR_TOGGLE" => DR is then used => LED is blinking.
Do you have any idea?
Hi Christian,
I was able to run tests with MCUXpresso10.2 + SDK2.4 + IMXRT1050-EVKB without problems.
Please let me know what tools and what versions are you using and please let me know how are you setting and clearing gpios.
Regards,
Carlos
Hi,
I use GPIO_PortSet, GPIO_PortClear and GPIO_PortToggl which use DR_SET, DR_CLEAR and DR_TOGGLE respectively.
Please note the following table:
SDK2.3.0 + IMXRT1050-EVK works but its deprecated
SDK2.3.0 + IMXRT1050-EVKB does not work
SDK2.3.1 + IMXRT1050-EVK does not work
SDK2.3.1 + IMXRT1050-EVKB works fine
SDK2.4 + IMXRT1050-EVK does not work
SDK2.4 + IMXRT1050-EVKB works fine
Hi
I am using Keil µVision MDK.
I have 4 boards, IMXRT1050-EVK and IMXRT1050-EVKB
I have tested the application ...\boards\evkbimxrt1050\driver_examples\gpio\led_output\mdk on both boards.
The application use the function "GPIO_PortToggle" for toggling the LED.
With macro "FSL_FEATURE_IGPIO_HAS_DR_TOGGLE" enabled the LED is !!! not !!! toggling, as i already mentioned.
The GPIO registers DR_SET, DR_CLEAR, DR_TOGGLE are not working correctly.