i.mx RT1050, USB Host -> Hub support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx RT1050, USB Host -> Hub support?

2,466 Views
dav1
Contributor V

Does any of the PHY's on the i.mx RT1050 support Hubs (in USB Host mode)?

thx /d

Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

1,981 Views
igorpadykov
NXP Employee
NXP Employee

Hi dav1

yes external usb hub can be connected to i.MXRT1050 usb host.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,981 Views
dav1
Contributor V

Hi Igor,

1. Just to clarify that we're talking "Multi-Point Support", i.e. that the USB controller when operating in host mode can host multiple USB peripheral devices. Please confirm.

2. How many end-points are supported?

3. Is there a driver or example project available, demonstrating multiple usb-devices running via a hub?

Thanks David

0 Kudos
Reply

1,981 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

one can look at usb examples in SDK

Welcome | MCUXpresso SDK Builder 

Best regards
igor

0 Kudos
Reply

1,981 Views
dav1
Contributor V

Hi Igor, I've done that, there is only very basic examples, no host with hubs.

Please reply my questions 1 & 2.

0 Kudos
Reply

1,981 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

number of endpoints is described in sect.55.1.1 Features

i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

For new questions suggest to create new thread.

Best regards
igor

0 Kudos
Reply

1,981 Views
dav1
Contributor V

from the "i.MX RT1050 Processor Reference Manual"

  • Up to 8 bidirectional endpoints

    Although there is no separate Transaction Translator block in the system, the transaction translator function normally associated with a USB 2.0 high speed hub has been implemented within the DMA and protocol engine blocks to support connection to full and low speed devices.

I've created a new topic for item 3:

https://community.nxp.com/message/1070835 

0 Kudos
Reply