i.mx 1050 CSI IP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx 1050 CSI IP

903 Views
natester
Contributor I

Hello,

I'm looking for details on the CSI IP Core in the i.mx1050. Specifically, is this IP shared with any other (more established) processors and can it be configured to support 2 cameras?

The data sheet describes the interface as a "Parallel CSI" interface, as opposed to the "Parallel Camera Port" and "MIPI CSI-2" interfaces on the i.mx 6

Thank you,

Nathan

Tags (1)
0 Kudos
2 Replies

774 Views
natester
Contributor I

Thanks Joan, I have reviewed this application note, however I do not see any more details on the source of the CSI IP block. Is it possible this IP block is shared with a more established device?

Best,

Nathan

0 Kudos

774 Views
joanxie
NXP TechSupport
NXP TechSupport

for camera module ,pls refer to the appication note as below:

https://www.nxp.com/docs/en/application-note/AN12110.pdf 

0 Kudos