i.MXRT1170 SEMC SDRAM Data Corruption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1170 SEMC SDRAM Data Corruption

Jump to solution
630 Views
george
Senior Contributor II

Hello All,

We are developing products using i.MX RT117x.
There seems to be something wrong with the behavior of SEMC with SDRAM, and we are investigating it now.


we found the following article.

https://community.nxp.com/t5/i-MX-RT/i-MXRT1060-SEMC-SDRAM-Data-Corruption/m-p/1169690

Should we do the same for the RT117x, whether or not it is related to the problem we have now?

BR,
George

 

Tags (1)
1 Solution
617 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Should we do the same for the RT117x, whether or not it is related to the problem we have now?
-- Yes, you can do it to get rid of reorder feature interference.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
618 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Should we do the same for the RT117x, whether or not it is related to the problem we have now?
-- Yes, you can do it to get rid of reorder feature interference.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
615 Views
george
Senior Contributor II

Hello @jeremyzhou,

Thank you for your quick reply.

We will consider whether to do that.

BR,
George