i.MXRT1020 EVK 24b RGB pins and usage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1020 EVK 24b RGB pins and usage?

Jump to solution
691 Views
fabio2
Contributor I

MIMXRT1020-EVK docs says that the i.MXRT1021 processor have 24 bits RGB interface but I can't find references of what pins are or software usage... Can help me to use it to handle a VGA monitor?

Labels (1)
0 Kudos
1 Solution
636 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Fabio,

 

Could you please provide which document stated that information? I believe this is a documentation error as there's no display support by default on the i.MXRT1020 EVK boards.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
637 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Fabio,

 

Could you please provide which document stated that information? I believe this is a documentation error as there's no display support by default on the i.MXRT1020 EVK boards.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
636 Views
fabio2
Contributor I

Hello, thank you for your answer. I search for where I saw that info and I believe I made a mistake with RT1050 info. Sorry about that

0 Kudos