i.MXRT ISP flashloader over Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT ISP flashloader over Ethernet

1,081 Views
chetkaufman
NXP Employee
NXP Employee

Is there an example for i.MXRT ISP boot loader for updating firmware that is downloaded over ethernet?  I see UART and USB are listed as supported by standard bootloader, but is there an example for Ethernet?

Labels (1)
0 Kudos
1 Reply

900 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Chet,

MCUXpresso SDK embedded MCU Bootloader doesn't provide Ethernet bootloader for RT1050.

I checked below resource for your reference:

Building and Self-Updating U-Boot on the NXP i.MX RT1050 EVK Board

Loading Linux Images via Ethernet and TFTP

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos