Is there an example for i.MXRT ISP boot loader for updating firmware that is downloaded over ethernet? I see UART and USB are listed as supported by standard bootloader, but is there an example for Ethernet?
Hi Chet,
MCUXpresso SDK embedded MCU Bootloader doesn't provide Ethernet bootloader for RT1050.
I checked below resource for your reference:
Building and Self-Updating U-Boot on the NXP i.MX RT1050 EVK Board
Loading Linux Images via Ethernet and TFTP
Wish it helps.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------