i.MXRT 1052 - External interrupt code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT 1052 - External interrupt code

584 Views
suhel_mulla
Contributor III

I am trying to use external interrupt on NXP i.MXRT 1050 EVK board.

I have following queries - 

1. Is there any code in the SDK for use of external interrupt ??

2. How I can configure the external interrupt on i.MXRT 1050 EVK board

3. Which APIs are required for the external interrupt configuration?

Labels (4)
0 Kudos
1 Reply

538 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Suhel,

 

I recommend you to check the igpio_input_interrupt example from the SDK that I believe it may be useful.

 

You can download the SDK from this link. Welcome | MCUXpresso SDK Builder

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 Kudos