i.MXRT 1010 How to execute code from RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT 1010 How to execute code from RAM

Jump to solution
1,886 Views
george_phang
Contributor I

Dear NXP Team,

I'm going to try put code running on RAM (not in external SPI) in Keil project,

but seem something Keil setting problem and unable build success.

 

Could you provide some example or teach me how to configure Keil setting? 

0 Kudos
1 Solution
1,865 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Sorry, I forgot to attach the file, so please check it now.
And you can learn more details by open the demo projects in the SDK library

Attachment.jpg
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

7 Replies
1,859 Views
george_phang
Contributor I

Hi,

 

Thanks your reply soon, I will test it right now.

So when I select to debug project, is that no need to download, just press start debug session? 

0 Kudos
1,845 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
1) Is that no need to download, just press start to debug session?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,839 Views
george_phang
Contributor I

Hi Jeremyzhou,

 Thanks you so much.

It's work.

0 Kudos
1,881 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could you provide some examples or teach me how to configure Keil setting?
-- Per the attachment, you can choose the flexspi_nor_polling_transfer_debug option to put code running on RAM.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,873 Views
george_phang
Contributor I

Hi, 

 

 R1. Per the attachment, you can choose the flexspi_nor_polling_transfer_debug option to put code running on RAM.

- I still not understand what I do in Keil project "flexspi_nor_polling_transfer"'s debug option.

0 Kudos
1,866 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Sorry, I forgot to attach the file, so please check it now.
And you can learn more details by open the demo projects in the SDK library

Attachment.jpg
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,875 Views
george_phang
Contributor I

Hi Jeremyzhou,

 

Thanks your reply, I would like to test attached Keil mdk project and run in RAM.

Could you help me to modify option?

 

Thanks a lots.

 

 

0 Kudos