i.MX rt1050 camera example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX rt1050 camera example

6,807 Views
thomasnielsen
Contributor II

Hi NXP.

I write to hear if any camera example code for the i.MX rt1050 is available?

Labels (1)
Tags (2)
12 Replies

4,706 Views
mingyang
Contributor I

Hi please let me the possible camera modules to use and if possible attach the link for me to purchase it too. In a rush, for an ongoing project that needs it. thank you.

0 Kudos
Reply

4,706 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Ming,

Here is the information for the company making the camera module:

http://gb.htkjks.com/

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply

4,706 Views
mingyang
Contributor I

current sdk supports mt7725?

0 Kudos
Reply

4,706 Views
mingyang
Contributor I

Hi Carlos,

thanks for the info. I would like to know the specific part no. I can purchase for mt9m114 and mt7725 which you recommended. Are 16 pin connectors to link the camera sensor to the i.mx rt1050 board included in my purchase?

0 Kudos
Reply

4,707 Views
mingyang
Contributor I

Hi, may i know what camera you are using for the i.mxrt1050.

What other cameras are compatible with the i.mx rt1050?

0 Kudos
Reply

4,707 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Ming,

i.MXRT1050 EVK designed with both MT9M114(720P) and MT7725(VGA).

And next SDK release will have MT9M114 support by default.

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply

4,707 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

In order to have the camera example working, you need to ensure your board version, considering the following note from “MIMXRT1050 EVK Extension Feature Enablement Guide” document:

note csi.png

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply

4,707 Views
thomasnielsen
Contributor II

Oh nice. The camera example was just made available in a user guide.

Thanks NXP :smileyhappy:
0 Kudos
Reply

4,707 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Thomas,

Yes, a camera example is included as “CSI” of the “i.MXRT1050 EVK Extended Feature Example Code and HW guide”, available at the link below:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

In case of requiring other examples, you could get the SDK for i.MX RT. For further details, take a look at the following thread:

https://community.nxp.com/thread/464274

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,707 Views
kyleyang
Contributor IV

Hi Carlos,

Thanks, but this Feature Example Code did not support MCUXpresso.

Is there any other document about porting the example code?

Thanks.

0 Kudos
Reply

4,707 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kyle,

At this time, just the mentioned examples are available, the "Extended Feature Example Code" package without MCUXpresso support, and the "SDK for i.MX RT", including MCUXpresso support.

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply

4,707 Views
stuartchen
Contributor I

Hi Carlos,

I have been concerned about this for a long time.

Will the official add the CSI example code for running on MCUXpresso IDE?

If yes, when is the schedule?

Thanks a lot.

Sincerely,

Stuart

0 Kudos
Reply