i.MX RT685 QSPI Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT685 QSPI Flash

2,190 Views
mark_wu
Contributor II

hello,

we choose a QSPI Flash(winbond W25Q64FWZPIG)for RT685, but failed to bring up.

flexspi_config:

pastedImage_1.png

  - ERROR: Failed to prepare RAMCode using RAM
  - ERROR: Error while determining flash info (Bank 0 @ 0x08000000)
  - ERROR: Failed to auto program target

we use FlexSPI PortA connect to flash,but in mcuxpressoide-11.1.1_3241/ide/binaries/Flash can't find the driver.

so how to config the flexspi?  tks

Labels (1)
Tags (2)
0 Kudos
1 Reply

2,123 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mark,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

To provide the fastest possible support, I'd highly recommend you refer to the attachment for details, the attachment is used to configure W25Q32JV.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos