i.MX RT1064 EVK PCB Files in Altium Format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1064 EVK PCB Files in Altium Format

1,808 Views
allthepies
Contributor I

Hi,

I have purchased the i.MX RT1064 EVK and would like to examine the PCB layout however I exclusively use Altium and I cannot import the design files which are in Cadence Allegro format.  Would it be possible to obtain a copy of the design files for this PCB in Altium format please?

Thanks,
Shane

Labels (1)
0 Kudos
7 Replies

1,535 Views
jaencer
Contributor I

They just send you the original Allegro files.  There is no Altium version.  We wound up re-designing the whole project in Altium.  

0 Kudos

1,588 Views
sagonzal
Contributor III

I'm in the same predicament, I've started to design a new board based on i.MX RT1064 and I only see Allegro files. We are in need of Altium files please. Kind regards.

0 Kudos

1,733 Views
jaencer
Contributor I

We need the same thing.  Are such files available?  

0 Kudos

1,739 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Shane,

I have contacted you via email.


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:

This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------

1,503 Views
azizsobaka
Contributor I

Hello! I am starting a new design using RT1064 and would like to know if there are Altium files for the design? If so can you please contact me? Thank you!

0 Kudos

1,539 Views
avbot
Contributor III

Hi, we urgently require these files also - please can you message us? Thank-you!

0 Kudos

983 Views
kksakthi
Contributor I
hi anyone received the IMXRT1064 altium file from NXP? Is it's possible to share me?
0 Kudos