i.MX RT1020, when will be available ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1020, when will be available ?

7,346 Views
luishs
Senior Contributor I

Hello

Does anyone know when the i.MX RT1020 will be available?

Regards

Labels (1)
0 Kudos
45 Replies

2,617 Views
mariocenteno
NXP Employee
NXP Employee

Samples of the 144LQFP are available now with production in Dec 2018.  Please contact your local distributor for samples.

0 Kudos

2,617 Views
614678489
Contributor I

what's the latest news of the 144LQFP package ? I want some samples right now !

0 Kudos

2,617 Views
mariocenteno
NXP Employee
NXP Employee

Hello Fun Lee,

Which region are you located in?  If you are located in China, please contact ZLG. They can get you i.MX RT1020 144LQFP samples.

thanks,

Mario

0 Kudos

2,617 Views
614678489
Contributor I

Or, could you please directly mail some 144LQFP samples to me ?

0 Kudos

2,617 Views
mariocenteno
NXP Employee
NXP Employee

Hello Fun,

We have samples today so let me put you in contact with our local team to get you samples.

thanks,

Mario

0 Kudos

2,617 Views
614678489
Contributor I

Gentleman, are you still there ? Could you please give me a cell phone number such that I can get some 144 LQFP samples ?

0 Kudos

2,617 Views
mariocenteno
NXP Employee
NXP Employee

Hello Fun,

Please look at your inbox for information on how to get samples.

thanks

Mario

0 Kudos

2,617 Views
614678489
Contributor I

Thanks a lot, I replied and somebody from Shanghai called me.

0 Kudos

2,617 Views
614678489
Contributor I

Gentleman, are you still there ?

My board is ready and just waiting for the 144 LQFP samples.......

0 Kudos

2,617 Views
614678489
Contributor I

Could you please give me a cell phone number in China such that I can get some 144 LQFP samples from there ? I wanna contact the REAL people with the REAL samples.

0 Kudos

2,617 Views
614678489
Contributor I

No one contact me as of yet.....

0 Kudos

2,617 Views
614678489
Contributor I

Thank you very much ! How will your local team contact me ? send me email or call my cell phone ? or, can I contact them instead ? Thanks again.

0 Kudos

2,617 Views
614678489
Contributor I

I checked with ZLG today, they only have 100LQFP, not 144LQFP at all, so, what should I do ? I am nervous.

0 Kudos

2,617 Views
614678489
Contributor I

Yes, I am in China, are you sure that ZLG has the 144 LQFP samples? Any other distributor in China can help me ?

0 Kudos

2,617 Views
luishs
Senior Contributor I

Any news about when the LQFP144 will be available?

0 Kudos

2,617 Views
luishs
Senior Contributor I

Can any NXP representative tell me when they will add Peripheral Tools to the SDK?. Are essential for me to be able to make new developments. Without the Peripheral Tools it is very difficult to configure DMA, interrupts, SPI, etc ...

0 Kudos

2,617 Views
luishs
Senior Contributor I

Just today, I received the 10 x RT1020 LQFP100 that I ordered from Digikey, very fast. I am ready to design my PCB for this powerful microcontroller, something easy with QSPI, SDIO, some leds for testing purposes and some additional chips and connectors for my LED screen application.

I hope that NXP will soon release a new version of the SDK with the Peripheral Tools for MCUXpresso, for me it is essential. Also I wait for the LQFP144, need it for some designs.

Time to migrate all my designs from Kinetis to RT1020.

RT1020_001.jpg

RT1020_002.jpg

0 Kudos

2,617 Views
arimendes
Contributor III

  I'm thinking of using the RT1020 instead of the STM32H7 in applications that do not need a high-performance ADC converter. But I do not understand why NXP did not made available any project examplos for the MIMXRT1020-EVK to be loaded directly into the external QSPI Flash. All the examples are for download and debug into the internal SRAM.

Ari 

0 Kudos

2,617 Views
bryancole-b4682
NXP Employee
NXP Employee

Hi Ari,

Most of the demo applications and driver examples that are included in the SDK for EVK-MIMXRT1020 have build configurations that target the QSPI. Are you using MCUXpresso IDE? You can import examples such as hello_world from the demo applications in the SDK which are targeted for the QSPI on the EVK.

0 Kudos

2,617 Views
luishs
Senior Contributor I

It seems that the RT1020 chip is now available to order (LQFP100 500Mhz), but only on Digikey, I ordered 10 units to test it and develop my new PCB, they will deliver them to me today by UPS. There are no free samples available on the NXP website.


I hope that it will soon be available also in Mouser (they announce it by the end of July), it is my preferred supplier for this type of product and, of course, the Chinese suppliers.


As for the SDK, it would be desirable, the sooner it support the Peripheral Tools, for me it is essential to configure the periphery, interrupts, DMA, etc ...

0 Kudos