i.MX RT minimal circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT minimal circuit

1,179 Views
paulson2003
Contributor I

Hello. I want to start programming the i.MX RT1064. But I need a minimal wiring of the microcontroller. Can you please continue to help me to give a circuit diagram(min. Schematic) with minimal wiring. Thank you.

0 Kudos
1 Reply

985 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Alex Kaboomski ,

Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the schematic of the MIMXRT1064, in addition, I've attached the schematic of Mini i.MX RT1052 and please check it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------