i.MX RT SEMC DQS Pin; Required or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT SEMC DQS Pin; Required or not?

1,496 Views
muratcakmak
Contributor II

Hi all,

In the i.MX RT1050 EVK SDRAM example, the project sets SEMC_DQS pin

IOMUXC_SetPinMux(IOMUXC_GPIO_EMC_39_SEMC_DQS, 1U); /* Software Input On Field: Force input path of pad GPIO_EMC_39 */

IOMUXC_SetPinConfig(
            IOMUXC_GPIO_EMC_39_SEMC_DQS, /* GPIO_EMC_39 PAD functional properties : */
            0x0110F9u); /* Slew Rate Field: Fast Slew Rate
            Drive Strength Field: R0/7
            Speed Field: max(200MHz)
            Open Drain Enable Field: Open Drain Disabled
            Pull / Keep Enable Field: Pull/Keeper Enabled
            Pull / Keep Select Field: Keeper
            Pull Up / Down Config. Field: 100K Ohm Pull Down
            Hyst. Enable Field: Hysteresis Enabled */

But this pin is not connected in the EVK schematic. We are now working on our board and this pin is used for a different purpose. If we configure the pin like above, SDRAM somehow works but we break the other functionality. 

It seems "Software Input On Field" is must otherwise the SDRAM does not work. But how a not-connected pin affects the SDRAM? Is there any internal mechanism for the SEMC module for SDRAM? If so, we might consider modifying the board which leaves the pin empty (or connected to the ground like as EVK)

Any idea? Thanks. 

Labels (1)
0 Kudos
2 Replies

1,268 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Murat Cakmak

Please see below table from the Reference Manual:

pastedImage_2.jpg

If you going to use the SEMC module, in some cases this pad needs a pull-down resistor, this is why this pin is configured with a pull-down resistor.

Hope this helps

Best regards

Jorge Alcala

0 Kudos

1,268 Views
muratcakmak
Contributor II

Thank you Jorge, just this pins is not connected to External SDRAM, does it still need a pull down resistor?

0 Kudos