i.MX RT 1064 Power up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT 1064 Power up

Jump to solution
2,038 Views
allen_tseng
Contributor I

Hi

I watched this thread https://community.nxp.com/t5/i-MX-RT/IMXRT1064-Power-Up-sequence/m-p/994938/thread-id/5905 .

And I have more question.

If I don't have a backup battery then the processor can connect all power at same time?

If it is yes, I can using only one LDO or converter without on-chip DCDC?

 

Allen

0 Kudos
1 Solution
2,000 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes. It is correct.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
2,027 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, if the lowest sleep power mode(SNVS Mode) is not necessary in your app, SNVS_IN can be POR together with other power domain to implement true one LDO or DC-DC regulator in system.

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
2,021 Views
allen_tseng
Contributor I

Hi fangfang

Thanks for your reply.

I referenced the "IMXRT1064CEC.pdf".

In chapter 4.1.1 Table.7 Absolute maximum ratings, I saw VDD_SOC_IN max 1.6V.

To simplify the power supply.

I think there are 2 way to achieve. Am I right?

1. one LDO-3.3V and using on chip DCDC conveter

2. one LDO-3.3V and one LDO-1.1V

 

I'm first using this type processor.

I was using simple MCU before.

Thanks for your patience.

 

Allen

0 Kudos
2,009 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I think there are 2 way to achieve. Am I right?

1. one LDO-3.3V and using on chip DCDC conveter

2. one LDO-3.3V and one LDO-1.1V.

For the RT application, Don't use one LDO-1.1V. Because VDD_SOC_IN is "Core supplies input voltage" .You may refer to the design for the EVK.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 
 

 

0 Kudos
2,005 Views
allen_tseng
Contributor I

Hi fangfang

Thanks for your reply.

For the RT application, Don't use one LDO-1.1V. Because VDD_SOC_IN is "Core supplies input voltage" .You may refer to the design for the EVK.

So I can using LDO-3.3V supply all processor power except VDD_SOC_IN.

And VDD_SOC_IN use internal DCDC to supply.

Is my understanding correct?

 

Allen

Tags (1)
0 Kudos
2,001 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes. It is correct.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos