Hey guys, I just received my new MIMXRT1015-EVK and encountered a problem during driver installation.
With the board connected to my win7 PC (LED was flashing), I ran the mbedWinSerial_16466.exe trying to install the driver:
I got "mbed Serail Port (COMxx)" installed correctly, but no luck with WebUSB: CMSIS-DAP.
as a result seems I was not able to probe the device via MCUXpresso.
I tried to re-run the driver installation, it gave "driver installed successfully" very soon, but nothing changed.
Rebooting the board/my PC didn't help.
Trying to manually uninstall "mbed Serail Port (COMxx)" and restarted the installation, now this interface also ran into problem.
Any idea what the problem would be? Thanks.
I figured it out, for some reason the driver installer exe wouldn't reinstall the driver.
But located them in below folder and manually installed it successfully.
C:\Program Files\mbed\drivers