Zephyr MIMXRT1050-EVK Ethernet support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Zephyr MIMXRT1050-EVK Ethernet support

跳至解决方案
1,411 次查看
jm2
Contributor I

Hi,

It seems that the MCUX Ethernet driver has not been enabled in the port of the mimxrt1050-evk to the Zephyr OS. I see that there is an active issue (#8900) in the zephyr project github to add this, can anyone tell me when we might expect it?

Thanks. 

0 项奖励
1 解答
1,214 次查看
maureen
NXP Employee
NXP Employee

Hi Jeremy,

We are starting to work on it now, so it will be available in the next release (1.14). You can subscribe to the GitHub issue to get an automatic notification when support gets merged into the upstream master branch.

Maureen

在原帖中查看解决方案

0 项奖励
1 回复
1,215 次查看
maureen
NXP Employee
NXP Employee

Hi Jeremy,

We are starting to work on it now, so it will be available in the next release (1.14). You can subscribe to the GitHub issue to get an automatic notification when support gets merged into the upstream master branch.

Maureen

0 项奖励