Hi
We want to use Winbond QSPI Flash W25Q256JVEIQ with the iMXRT1172.
Is the above flash part W25Q256JVEIQ compatible for iMXRT1172 QSPI flashing? if yes, will the flash W25Q256JVEIQ will be able to support XIP mode and Secure architecture mode for iMXRT1172?
Please let us know. Any support on the above query will be really helpful
Thanks and Best Regards,
Vihang Waze
Design Engineer
TATA ELXSI Limited
Solved! Go to Solution.
Hi @vihang_vinayak ,
Yes, W25Q256JVEIQ is able to support XIP mode and Secure architecture mode for iMXRT1172.
https://community.nxp.com/t5/i-MX-RT/RT105x-boot-from-QSPI-W25Q256JV/m-p/1173455
Regards,
Jing
Hi @vihang_vinayak ,
Yes, W25Q256JVEIQ is able to support XIP mode and Secure architecture mode for iMXRT1172.
https://community.nxp.com/t5/i-MX-RT/RT105x-boot-from-QSPI-W25Q256JV/m-p/1173455
Regards,
Jing