Wifi - how to enable 802.11e (QoS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wifi - how to enable 802.11e (QoS)

Jump to solution
577 Views
h_bouchard
Contributor III

Hello,

We are using the PAN9026 module along with NXP SDK 2.9.1.

We are transferring voice data over WiFi and would like to enable the 802.11e protocol. I know that PAN9026 supports it. I can see that LWIP also supports this. However, I don't see how to enable it in the PAN9026 using Wifi module of NXP SDK. I see a lot of IOCTL functions in mlan_ioctl.h and other functions in mlan_glue.c but I don't know which one (if any) to use.

Can someone help?

Regards,
Hugo

Labels (2)
Tags (3)
0 Kudos
1 Solution
558 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @h_bouchard,

Unfortunately, the only device right now that supports WMM is the 88W8987 but there's been some major changes in the Wi-Fi SDK since the 2.9.1, the latest one is the 2.11.1 and there's been changes between these two versions that could improve the performance.

BR,

Alexis Andalon

View solution in original post

0 Kudos
1 Reply
559 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @h_bouchard,

Unfortunately, the only device right now that supports WMM is the 88W8987 but there's been some major changes in the Wi-Fi SDK since the 2.9.1, the latest one is the 2.11.1 and there's been changes between these two versions that could improve the performance.

BR,

Alexis Andalon

0 Kudos