Wi-Fi / BT solutions for RT 1060 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wi-Fi / BT solutions for RT 1060 evk

Jump to solution
2,136 Views
romitchatterjee
Contributor V

Hello, looking for a Wi-Fi + BT solution for NXPs i.MX RT 1060 evk. It does not seem to come with Wi-Fi/BT built-in? Any suggestions?

Best regards,

Romit Chatterjee 

Labels (1)
1 Solution
1,897 Views
puja_sah
Contributor II

Hello Romit,

You can use Murata's M.2 module (i.e. Wi-Fi+BT combo solution) for the i.MX RT board. There are three M.2 modules i.e Type 1DX, Type 1LV and Type 1MW EVB which are compatible with NXP's i.MX RT 1060 EVK. Till now NXP SDK only includes support for 1DX and 1LV modules. Type 1MW is scheduled to be included in their upcoming release. Please refer to the links below to learn more about our M.2 modules:

https://wireless.murata.com/type-1dx.html

https://wireless.murata.com/type-1lv.html

https://wireless.murata.com/type-1mw.html

Also, here is the link to the quick start guide to get started with i.MX RT 1060 using M.2 modules:

https://wireless.murata.com/pub/RFM/data/murata_quick_start_guide_freertos.pdf

Thanks,

Puja

View solution in original post

4 Replies
1,896 Views
romitchatterjee
Contributor V

Thanks Tomohiro san, Puja and Markus! Much appreciated for your answers. These should be enough for now to get me started.

Best regadrs,

Romit

0 Kudos
1,897 Views
Masmiseim
Senior Contributor I

Hello Romit,

 

NXP is using “SX-ULPAN-2401-SHIELD” and “Murata 1DX M.2 module” in there SDK-Examples. Maybe this could be a good starting position.

 

Best Regards

1,898 Views
puja_sah
Contributor II

Hello Romit,

You can use Murata's M.2 module (i.e. Wi-Fi+BT combo solution) for the i.MX RT board. There are three M.2 modules i.e Type 1DX, Type 1LV and Type 1MW EVB which are compatible with NXP's i.MX RT 1060 EVK. Till now NXP SDK only includes support for 1DX and 1LV modules. Type 1MW is scheduled to be included in their upcoming release. Please refer to the links below to learn more about our M.2 modules:

https://wireless.murata.com/type-1dx.html

https://wireless.murata.com/type-1lv.html

https://wireless.murata.com/type-1mw.html

Also, here is the link to the quick start guide to get started with i.MX RT 1060 using M.2 modules:

https://wireless.murata.com/pub/RFM/data/murata_quick_start_guide_freertos.pdf

Thanks,

Puja

1,898 Views
TomohiroInoue
Contributor II

Hi Romit,

The SDK 2.5.1 supports Murata Type1DX Wifi/Bluetooth combo module if you add additional components (basically 'select all' helps) when you download the SDK.

You can check our quick start guide to learn more about the details: https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf

Here is the adapter board information: https://wireless.murata.com/usd-m2

Here is the stock information for the adapter board: https://www.eciaauthorized.com/en/search/LBEE0ZZ1WE

Here is the stock information for the 1DX M.2 Module board: https://www.eciaauthorized.com/en/search/EAR00318

Best regards,

Tom Inoue