Why can't change the OCRAM size?

cancel
Showing results for 
Search instead for 
Did you mean: 

Why can't change the OCRAM size?

435 Views
diangongcxq
Contributor II

I was using the rt1020-evk board.I change the OCRAM size from 128KB to 64KB,but the program will enter hardFault before starting main function.

The minimum configuration of OCRAM is 64 KB according to datasheet,but i failed to change that.

So i need your help.

Thanks.

0 Kudos
1 Reply

323 Views
FelipeGarcia
NXP TechSupport
NXP TechSupport

Hi,

 

Please make sure you are also reconfiguring IOMUXC_GPR_GPR17 register during the startup. Please check this link where my colleague gives a detailed description of how you can accomplish this.

Hope it helps!

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

- Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------