Why PN5180 card detcet dosen't reponse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why PN5180 card detcet dosen't reponse

1,312 Views
yen_chen
Contributor III

Hi,

I use NFC module Pn5180 with MCU soc RT1050.

Now in the LPCD function  ,we need to detect card and it will wait IRQ happen.

yen_chen_0-1625126919847.png

yen_chen_1-1625126957728.png

 In the demo kit sample LPC1769 with PN5180 ,detect card and it will send data.

But in the RT1050 with PN5180, detect card it doesn't response any data and it will keep in function phOsal_Sleep() .

yen_chen_2-1625127346917.png

Our DAL and phApp_init.c the attachment .

Please help me check that setting whether it right or not?

 

 

 

 

 

0 Kudos
2 Replies

1,302 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello.

One may refer to the NFC library of PN5180 as the path SW352228\NxpNfcRdLib_PN5180_v06.10.00_Full\Examples\NfcrdlibEx6_LPCD.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos

1,293 Views
yen_chen
Contributor III

HI @fangfang 

I have RF status issue

yen_chen_2-1626178238977.png

 

After SwitchModeLpcd RF status not same the demo kit.

read RF status register

yen_chen_0-1626178170136.png

 

demo kit RF status : 0,74,1,50

our RF status :0,4,1,50

 

and Int_ActivePollMode

yen_chen_1-1626178205966.png

 

demo kit RF status

1.  0,74,1,50

2. 0,76,0,87

3. 1,76,0,86

....

our RF status

1. 0,4,1,50 (TYPE_P2P_ACTIVE)

2. 0,56,1,29 (Sw_Int_FieldOn)

3. 1,46,1,59 (Send ATR Request)

and it wll get stuck here.

Is the RF driver have some problem?

 

0 Kudos