Using the iMXRT1020 OTP memory to store manufacturing data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the iMXRT1020 OTP memory to store manufacturing data?

885 Views
ashishpradhan
Contributor II

Hi,

We would like to use the OTP (iMXRT1020) to store some of our production/manufacturing data. Would like to know which OTP regions are safe to write to? 

The IMXRT1020 reference manual lists the OTP memory footprint as shown below. Could not find information in manual regarding which OTP regions can be used for storing manufacturing data.  

We have about 60 bytes of manufacturing info that we need to store on OTP. Can we use MEM, SW_GP,GP2 and MAC regions to store the info?

Our product does not have a MAC address so, can the MAC region be used to store some other data viz. serial number instead of MAC address?

OTP.png

Regards,

Ashish

Labels (1)
0 Kudos
3 Replies

733 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ashish Pradhan,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Q1) Can we use MEM, SW_GP, GP2 and MAC regions to store the info?
-- Yes, you can use the fields except for the MEM field, as the MEM field is reserved section.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

733 Views
ashishpradhan
Contributor II

Thank you jeremyzhou‌ for the quick response.‌

Can we also use ANALOG and MISC_CONF sections?

Regards,

Ashish

0 Kudos

733 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ashish Pradhan,

Thanks for your reply.
1) Can we also use ANALOG and MISC_CONF sections?
-- I'm afraid you can't do that.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos