Using rt1050 flexpwm X output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using rt1050 flexpwm X output

4,221 Views
peter_lombrozo
Contributor IV

We have a hardware configuration that requires putting a PWM signal on the Flexpwm1 output X pin (GPIO_AD_B0_03).  I can get the SDK PWM example to put a PWM on A or B outputs, but not the X output.  I can't seem to make the PWM drivers access that pin for the pwm signal.  How do I configure the FlexPWM1 module, submodule 1 to do this?  Thanks.

Labels (2)
0 Kudos
Reply
3 Replies

3,902 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Peter Lombrozo,

   GPIO_AD_B0_03 can be used as flexpwm1.

pastedImage_3.png

Do you modify the pin_mux.c to configure the pin function?

If you already modify it, and it still can't work.

Please tell me the details about your modified code based on the SDK, then I will help you to check it.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,902 Views
peter_lombrozo
Contributor IV

Yes, I had the pin mux correct.  The problem is that the PWM_X channel is not available in the SDK drivers.  However, I got it to work by modifying fsl_pwm.c,h to configure PWM_X that creates a new mode that was not aligned and disabling the deadband.

fsl_pwm.c
10c10
<
---
387a388,396
> case kPWM_NonAligned:
> /* Setup the PWM period for a PWM_X non-aligned signal */
> /* Indicates the start of the PWM period */
> base->SM[subModule].INIT = 0;
> /* Indicates the center value */
> base->SM[subModule].VAL0 = (pulseCnt / 2);
> /* Indicates the end of the PWM period */
> base->SM[subModule].VAL1 = pulseCnt;
> break;
400c409
< else
---
> else if (chnlParams->pwmChannel == kPWM_PwmB)
448c457
< assert(pwmSignal < 2);
---
> assert(pwmSignal < 3);
521a531,543
> }
> break;
> case kPWM_NonAligned: // Only for PWM_X output
> pulseCnt = base->SM[subModule].VAL1;
> /* Calculate pulse width */
> pwmHighPulse = (pulseCnt * dutyCyclePercent) / 100;
> if (pwmSignal == kPWM_PwmX)
> {
> base->SM[subModule].VAL0 = pwmHighPulse;
> //base->SM[subModule].VAL1 = ;

fsl_pwm.h

230c230,231
< kPWM_EdgeAligned /*!< Unsigned edge-aligned */
---
> kPWM_EdgeAligned, /*!< Unsigned edge-aligned */
> kPWM_NonAligned /*!< Not aligned for PWM_X channel*/

0 Kudos
Reply

3,902 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Peter Lombrozo,

    Thanks a lot for your updated information.

    And thank you for the modified point sharing.

   Now, after the modification, do you still have any problem about it?

  If you still have the problems, please kindly let me know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply