Using USB to Ethernet converter with iMX RT 1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB to Ethernet converter with iMX RT 1050

Jump to solution
1,057 Views
audio
Contributor III

Hello,

I have seen some information that we can directly connect an external ethernet cable to iMX RT 1050, using a USB to Ethernet(RJ-45) converter.Can we use any kind of USB to Ethernet converter for the iMX RT MCUs? I have found that the most compatible configuration is the ECM(Ethernet Control Model) for most of the devices.
Also, are they any examples of processing ethernet over USB?

 

Thank You

 

0 Kudos
1 Solution
1,050 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The i.MXRT should be the USB Host with CDC support. On the MCUXpresso SDK v28.0 for EVKB-MIMXRT1050, it is available an example with such characteristics under “usb_examples->host_cdc_bm”.
This example asks for a USB-UART Device, so, it will be required applying the proper changes to work with USB-Ethernet and with the desired functionality.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

View solution in original post

1 Reply
1,051 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The i.MXRT should be the USB Host with CDC support. On the MCUXpresso SDK v28.0 for EVKB-MIMXRT1050, it is available an example with such characteristics under “usb_examples->host_cdc_bm”.
This example asks for a USB-UART Device, so, it will be required applying the proper changes to work with USB-Ethernet and with the desired functionality.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------