Using RPMSG to communicate between cores with different OS's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using RPMSG to communicate between cores with different OS's

1,807 Views
D_TTSA
Contributor V

Good day

I would like to communicate between the  M4 and M7 cores on the RT117-EVK.

However, I am running BareMetal OS on the M4 and FreeRTOS on the M7. This operating system selection cannot be changed due to my project's constraints.

I can communicate between the two cores using RPMSG if they are using the same operating system (by creating my own project that mimics either the rmpsg_lite_pingpong_ example or the rpmsg_lite_rtos_pingpong_ example. 

But as soon as I change the operating system (and the RPMSG middleware component) from BareMetal to FreeRTOS on the M7, the communication does not work. The master (M7) gets stuck in the second while loop in the image below:

D_Tram23_0-1623142529865.png

Please let me know if someone knows how to fix this.

0 Kudos
Reply
5 Replies

1,802 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need to know more information about the question, so I was wondering if you can introduce the code modifications you did
Looking forward to your reply.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,798 Views
D_TTSA
Contributor V

@jeremyzhou , thank you for your response.

I used the evkmimxrt1170_rpmsg_lite_pingpong_cm4 and _cm7 main files and rpmsg_config.h files (which are the Baremetal SDK example) as the base for my modifications.

First, let me clarify exactly what my problem is so that you understand the slight modifications I made. The following line, in main_remote.c, executes as expected on the M4 (returns kStatus_MCMGR_Success), but this event is not picked up by the master:

D_Tram23_0-1623219963324.png

As a result, the main_master.c debug never leaves this while loop:

D_Tram23_1-1623220034343.png

Based on the evkmimxrt1170_rpmsg_lite_pingpong_rtos_cm4 and _cm7 example files (FreeRTOS SDK example), it seems that FreeRTOS uses RPMSG's nameservice component instead of the above event trigger. Based on this assumption, I copied the code to integrate this from the SDK example into my main_master.c:

D_Tram23_2-1623220356381.png

and main_remote.c:

D_Tram23_3-1623220400328.png

I had to modify these function calls slightly - I included the context variables as the last argument for the calls, because the rpmsg_config.h files define RL_USE_STAT_API as 1 (to stay in line with the Baremetal SDK example). However, I don't think this matters, because these are output variables for the functions, I think. Anyway, this has the same result as the aforementioned event, as the main_master.c debug never leaves the while loop (remote_addr is not changed).

I think the best way to replicate what I'm trying to do is to try to use the evkmimxrt1170_rpmsg_lite_pingpong_cm7 example project (converted to FreeRTOS) to control with the evkmimxrt1170_rpmsg_lite_pingpong_cm4 (Baremetal) example project. Another option is to use evkmimxrt1170_rpmsg_lite_pingpong_rtos_cm7 as the master project and adjust it to control evkmimxrt1170_rpmsg_lite_pingpong_cm4 - I have tried this too. As explained above, my modifications have had no effect, so I don't mind leaving them out.

0 Kudos
Reply

1,788 Views
D_TTSA
Contributor V

My colleague found the problem. The FreeRTOS master project's code must be placed in a task, and started by calling 'vTaskStartScheduler()'. Previously, my code was running directly in main().

If a task is used, then the two cores communicate via RPMSG as one would expect.

However, I'm not going to close this thread yet, as I would like an explanation for why this is the case? As far as I understand from the FreeRTOS reference manual, the code in main() is run just like the code in a task, before any tasks are started by the scheduler:

D_Tram23_0-1623239347272.png

 

Clearly, vTaskStartScheduler() is doing something in the background that I am not aware of.

@jeremyzhou are you aware of why this would be the case?

0 Kudos
Reply

1,779 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Sorry for reply late.
It seems a bit weird, maybe you can try to move out the the code of the app_task in evkmimxrt1170_rpmsg_lite_pingpong_rtos_cm7 demo and run it just like the BareMetal version does, even though the demo has already intergrated the FreeRTOS.
Note: Don't do any code modification except for above moving out action.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,775 Views
D_TTSA
Contributor V

Hi @jeremyzhou 

As stated above, I have fixed it, but I would like to know the reason why there is an interaction between RPMSG and FreeRTOS's vTaskStartScheduler.

0 Kudos
Reply