Examples: evkmimxrt1064_lwip_httpssrv_ota_enet AND evkmimxrt1064_ota_demo_enet
require MCUBoot bootloader.
RT1064 has ROM bootloader, but am I understanding correctly that these demos need custom version of MCUBoot bootloader programmed into Flash to run?
Text from demo app readme:
"The demo requires MCUBoot bootloader to be present in the FLASH memory to function properly.
It is recommended to build and program the bootloader first, then go on with the application.
Please refer to respective readme of the mcuboot_opensource example "
Please provide the source for MCUBoot bootloader for RT1064 as soon as possible.
解決済! 解決策の投稿を見る。
Thanks.. actually I just found it in 1064 SDK 2.12, feature needs to be configured first.
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) RT1064 has ROM bootloader, but am I understanding correctly that these demos need custom version of MCUBoot bootloader programmed into Flash to run?
-- Yes.
2) You can find the demo of mcuboot_opensource resides ~\boards\evkbmimxrt1060 of SDK library.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks.. actually I just found it in 1064 SDK 2.12, feature needs to be configured first.